Technical FAQs

Ask a Question

What actions should I take upon seeing an ECxx error?

 
 

 In the event that you encounter an ECxx error, you must perform the following action.

  Power cycle the PLC exactly one time.
  Connect to the PLC with Unity
  Select Help\About Unity Pro\ Technical Support
  Generate the file and send it along to Technical Support.
  The file will be sent to R&D for further analysys


 After performing the previous step you can attempt to recover the PLC by performing a download of the application.

  Finally, if the ECxx error is repeatable you should replace the CPU.


 



 

text

Legacy KB System (APS) Data: RESL212325 V1.0, Originally authored by DaSo on 08/16/2013, Last Edited by DaSo on 08/16/2013
Related ranges: Modicon Quantum
Was this helpful?
What can we do to improve the information ?