Technical FAQs

Ask a Question

How do I eliminate a "configuration binary generation" error when making on-line modifications with Unity Pro.

This error has been seen only a handful of times using 6.0 and 6.1. On one occasion it was resolved by manually entering a variable name instead of using copy - paste. In all other cases, the solution was to perform a 'build all' and full down load when the opportunity allows.


Legacy KB System (APS) Data: RESL212322 V1.0, Originally authored by DaSo on 08/16/2013, Last Edited by DaSo on 08/16/2013
Related ranges: Unity Pro - SoCollaborative software
Was this helpful?
What can we do to improve the information ?