Technical FAQs

Ask a Question

Unity Pro V6.0 is displaying a "The DTM device is not found." message when adding a '140 CRP 312 00' to the Local Bus.

This means that the DTM catalog needs to be updated. Open the Hardware Catalog either by pressing ALT+2 or from the Tools menu. At the bottom of the Hardware Catalog select the DTM Catalog tab. Now you will see two buttons, 'External Update Tool' and 'Reload catalog'. First select the External Update Tool and this will open the FDT/DTM catalog window. Press the update button located in the lower left hand corner of this window, this will update the catalog and it could take a few minutes. Upon completion a message will tell you that the Update is completed and a reload is necessary, acknowledge that message and then close the update window. Now you are back to the Hardware Catalog window. Select the Reload catalog button and once complete, you should be able to go back and select the 140 CRP 312 00 in the local bus.


Legacy KB System (APS) Data: RESL212319 V1.0, Originally authored by DaSo on 08/16/2013, Last Edited by DaSo on 08/16/2013
Related ranges: Unity Pro - SoCollaborative software
Was this helpful?
What can we do to improve the information ?