Technical FAQs

Ask a Question

Is function 15 for the MBP_MSTR block supported with a 140CPU43412U PLC?

Yes.
MBP_MSTR function code 15 has the following requirements at minimum;
NOE77101 version 5.0
NOE77111 version 5.0
Unity Quantum CPU (includes 534 and 434) Exec firmware version 3.0
Unity 6.0
The CPU native Ethernet port or MB+ ports do not support this function, NOE only.

 
text

Legacy KB System (APS) Data: RESL212318 V1.0, Originally authored by DaSo on 08/16/2013, Last Edited by DaSo on 08/16/2013
Related ranges: Unity Pro - SoCollaborative software
Was this helpful?
What can we do to improve the information ?