Technical FAQs

Ask a Question

Can the Concept simulator run a program that has IO scanner configured and have that IO scanner access external Modbus TCP devices?

No. IO Scanner functionality is not supported with the Concept Simulator.


Legacy KB System (APS) Data: RESL212294 V1.0, Originally authored by DaSo on 08/12/2013, Last Edited by DaSo on 08/12/2013
Related ranges: Concept
Was this helpful?
What can we do to improve the information ?