Technical FAQs

Ask a Question

If we have a Unity Quantum hot standby system, is it possible to take one processor off-line to make a default gateway change? Then put it back on line, fail over to it, then take the other one down and change that one?

No. This constitutes a configuration change that is not supported.


Legacy KB System (APS) Data: RESL212289 V1.0, Originally authored by DaSo on 08/12/2013, Last Edited by DaSo on 08/12/2013
Related ranges: Modicon Quantum
Was this helpful?
What can we do to improve the information ?