Technical FAQs

Ask a Question

Connecting to a Momentum's Modbus port#2 RS485 DB9 port using a TSXCUSB485 adapter for programming

Goals and Symptoms


Connecting to a Momentum Modbus port#2 RS485 DB9 port using a TSXCUSB485 adapter for programming…..

Causes and Fixes



Connecting to a Momentum RS485 DB9 port using a TSXCUSB485 adapter for programming…..




**** When connecting to the RS485 port of the Momentum processor with the wiring scheme above only Positions 0 and 1 on the adapters rotary wheel will allow you to connect to the processor…


Was this helpful?
What can we do to improve the information ?