Technical FAQs

Ask a Question

What is the recommended maximum torque for the screws on the TSX Momentum 170XTS00100 connector?

The recommended maximum torque for the screws on the TSX Momentum 170XTS00100 connector is 4.4 in/lb (0.5 Nm)


Legacy KB System (APS) Data: RESL212137 V1.0, Originally authored by RoAl on 07/24/2013, Last Edited by RoAl on 07/24/2013
Related ranges: Modicon Momentum
Was this helpful?
What can we do to improve the information ?