Technical FAQs

Ask a Question

Is there a PowerSuite version that is compatible with Win7 64 bit platform?

Patch 3 for PowerSuite version 2.6.0 supports Win 7 32 bit. Thus it is not compatible with Win 7 64 bit O/S.
Patch 3 supports Windows versions

Vista Sp1
Vista Sp2
Win 7 32 bit

Note : Installation can be done only in administrator mode.


Legacy KB System (APS) Data: RESL212117 V1.0, Originally authored by TVe on 07/23/2013, Last Edited by TVe on 07/23/2013
Related ranges: PowerSuite
Was this helpful?
What can we do to improve the information ?