Technical FAQs

Ask a Question

Is the Serial Cable for the LINK150 ( VW3A8306D30) UL Certified?

Issue:
End User may need know if the LINK150 serial cable  (VW3A8306D30) is UL certified

Product Line:
LINK150

Environment:
Serial Communications Cable 

Cause: 
Some projects might require that all parts of a system or design must be UL certified. 

Resolution: 
VW3A8306D30 is a communication cable and is not UL Certified as it is a LOW_VOLTAGE cable. The same applies to all our communication cables as well.
 


Legacy KB System (APS) Data: RESL212095 V1.0, Originally authored by TVe on 07/19/2013, Last Edited by TVe on 07/19/2013
Related ranges: Other VVD PRODUCTS
Was this helpful?
What can we do to improve the information ?