Technical FAQs

Ask a Question

Do the Magelis terminals support PROFINET protocol for communication with Siemen's controllers?

None of the Magelis terminals support PROFINET protocol. Ethernet/Modbus TCP is the only available mode of communication with Siemen's PLCs.


Legacy KB System (APS) Data: RESL212083 V1.0, Originally authored by TVe on 07/18/2013, Last Edited by TVe on 07/18/2013
Related ranges: Magelis XBT GT
Was this helpful?
What can we do to improve the information ?