Technical FAQs

Ask a Question

Is there any repair or exchange available for the Sy/Max Model 50?

The Sy/Max Model 50 is obsolete and no longer available since 6/1/10. There is no repair or exchange on this product - an upgrade is required.


Legacy KB System (APS) Data: RESL212048 V1.0, Originally authored by DiSa on 07/12/2013, Last Edited by DiSa on 07/12/2013
Related ranges: Sy/Max
Was this helpful?
What can we do to improve the information ?