Technical FAQs

Ask a Question

Is the TSX Momentum 171CCC76010 CPU compatible with the 170INT11000 Interbus Communication Adapters?

Yes. the TSX Momentum 171CCC76010 CPU is compatible with the 170INT11000 Interbus Communication Adapter. You will need the programming software to add the configuration in.


Legacy KB System (APS) Data: RESL212044 V1.0, Originally authored by DiSa on 07/12/2013, Last Edited by DiSa on 07/12/2013
Related ranges: Modicon Momentum
Was this helpful?
What can we do to improve the information ?