Technical FAQs

Ask a Question

I am attempting to re-install Advantys V7.0 after a complete un-install. Why am I getting a "the installer was interrupted before Advantys could be completely installed" message?

One possible cause is that there are remnants from the previous install in the registry. One of the main culprits of this message is the Advantys folder located under HkeyLocalMachine>Software>Schneider Electric. Find and delete this folder then re-attempt the install.


Legacy KB System (APS) Data: RESL212008 V1.0, Originally authored by DaSo on 07/09/2013, Last Edited by DaSo on 07/09/2013
Related ranges: Modicon STB
Was this helpful?
What can we do to improve the information ?