Technical FAQs

Ask a Question

What is the part number for the circuit board only of a Quantum backplane ?

There is no part number for the circuit board only of a Quantum backplane. The entire backplane would have to be exchanged or returned.

Was this helpful?
What can we do to improve the information ?