Technical FAQs

Ask a Question

What are the specifications of the Fiber optic cables used with SERCOS Motion Controllers and drives?

Goals and Symptoms

The purpose of this resolution is to inform the user of specifications of the fiber optic cables specified by Schneider Electric for its Motion Control Solution.

Causes and Fixes

The fiber optic cables that are used with the Quantum SERCOS Motion Controllers and associated SERCOS compatible Cyberline and Lexium drives are SMA plastic cables. They are equipped with FSMA type connectors on either end. IEC 1491 SERCOS specification states that either glass or plastic fiber optic cables may be used. Schneider fiber optic cable is 1mm plastic fiber and has an attenuation of 220 dB/km. The cables have been fully qualified with the Schneider Motion control System. Schneider does not offer these fiber optic cables as the product range is obsolete.

Schneider makes no recommendations on the use of repeaters and none have been qualified with Schneider's motion control system.


Legacy KB System (APS) Data: RESL211948 V1.0, Originally authored by TVe on 07/03/2013, Last Edited by TVe on 07/03/2013
Related ranges: Other Motion controllers, Modicon Quantum (Motion), Lexium 17D
Was this helpful?
What can we do to improve the information ?