Technical FAQs

Ask a Question

What is the part number for the Lexium23 programming cable?

The part number for the Lexium23 programming cable (two piece cable) is: VW3M8131 (USB to RJ45(RS232) converter forCN3 interface) + 490NTW00002 (standard network cable)


Legacy KB System (APS) Data: RESL211924 V1.0, Originally authored by TVe on 06/28/2013, Last Edited by TVe on 06/28/2013
Related ranges: Lexium 23
Was this helpful?
What can we do to improve the information ?