Technical FAQs

Ask a Question

What are the pinouts for current inputs on the AMI0810 when using the FTW308 cable with pigtail leads ?

 

 

 
  : Here are the pin assignments for current inputs I0 - I7 when using the FTW308 cable and the BMXAMI0810 .
 
      
    Current input 0  +                   pins 1/3 blue/white & white/blue are jumped together
    Current input 0  common        pin 2 white/orange
 
    Current input 1  +                   pins 4/6  green/ white & white/green are jumped together
    Current input 1  common        pin 5 orange/white
 
    Current input 2  +                   pins 7/9 white/brown  & brown/white are jumped together
    Current input 2  common        pin 8   white/gray 
 
    Current input 3  +                   pins 10/12 blue/red & red/blue are jumped together
    Current input 3  common        pin 11 gray/white
 
    Current input 4  +                   pins 15 /17 red/ orange & orange/ red are jumped together
    Current input 4  common        pin 16 red/green
 
    Current input 5  +                   pins 18/20 brown/red & red/brown are jumped together
    Current input 5  common        pin 19 green/red  
 
   Current input 6  +                 pins 21/23 red/gray & gray/ red are jumped together
   Current input 6  common        pin 22 black/blue
 
   Current input 7  +                   pins 24/26 black/orange & orange/ black are jumped together
   Current input 7  common        pin 25 blue/black 


R-6-30-17

Legacy KB System (APS) Data: RESL211859 V1.0, Originally authored by DaSo on 06/21/2013, Last Edited by DaSo on 06/21/2013
Related ranges: Modicon M340
Was this helpful?
What can we do to improve the information ?