Technical FAQs

Ask a Question

Is there a list of blocks used in Concept that are not included as part of the Concept to Unity conversion?


Yes, and in addition to the following list you can also include SCALRTOW and SCALWTOR..


Legacy KB System (APS) Data: RESL211858 V1.0, Originally authored by DaSo on 06/21/2013, Last Edited by DaSo on 06/21/2013
Related ranges: Unity Pro - SoCollaborative software
Was this helpful?
What can we do to improve the information ?