Technical FAQs

Ask a Question

Does the M340 NOE I/O Scanner have a Device Control Block similar to the Quantum I/O Scanner?

The M340 NOE does not incorporate the Device Control Block in the same way as the Quantum NOE does VIA the IO Scanner configuration table. There is an IODDT available for the module that provides the Device Control Block functionality along with other status bits. A variable of data type T_COM_ETH_BMX must be created. Detailed information on this IODDT can be found in the Unity online help.


Legacy KB System (APS) Data: RESL211849 V1.0, Originally authored by MiMe on 06/20/2013, Last Edited by MiMe on 06/20/2013
Related ranges: Modicon M340
Was this helpful?
What can we do to improve the information ?