Technical FAQs

Ask a Question

Are there limitations of Quantum power supplies installed in a backplane?

Quantum powers supplies are available in 3 models / types Standalone, Summable and Redundant
A Standalone power supply cannot be combined in a backplane with any other model / type.
Summable and Redundant power supplies cannot be mixed in the same backplane.
The Quantum Hardware Reference Manual (840USE10000) Appendix D has detailed information on Power and Grounding Guidelines.

Legacy KB System (APS) Data: RESL211823 V1.0, Originally authored by DiSa on 06/17/2013, Last Edited by DiSa on 06/17/2013
Related ranges: Modicon Quantum
Was this helpful?
What can we do to improve the information ?