Technical FAQs

Ask a Question

What is the extended operating temperature range of the M340 Processors?

The extended operating temperature range of the M340 Processors is from -25 degree Celsius to 70 degree Celsius.


Legacy KB System (APS) Data: RESL211794 V1.0, Originally authored by TVe on 06/14/2013, Last Edited by TVe on 06/14/2013
Related ranges: Modicon M340
Was this helpful?
What can we do to improve the information ?