Technical FAQs

Ask a Question

Preventa XY2C - XY2CH rope pull switch - Reset not possible at product delivery, without cable : is it a quality issue?

This XY2C* switch behaviour is normal for switches dedicated for E. stop function with a reset button. It is necessary to install the cable for tripping, and adjust it correctly according to the user manual or instruction sheet, in order to operate the reset function of the switch. This is not a quality trouble of the product.


Legacy KB System (APS) Data: RESL211778 V1.0, Originally authored by JeLe on 06/13/2013, Last Edited by JeLe on 06/13/2013
Related ranges: Preventa XY2C
Was this helpful?
What can we do to improve the information ?