Technical FAQs

Ask a Question

Can I use the PCFL_AIN block with M340 analog IO?

Yes, you can use the PCFL_AIN block with M340 analog IO. However, you will experience better resolution and scaling capability by using the BMXAMx xxx onboard scaling found in the module's configuration screen. If you feel the need to modify your scaling attributes while online, consider using the SCALING block with your BMXAMx xxx rather than PCFL_AIN
for M340 applications


Legacy KB System (APS) Data: RESL211748 V1.0, Originally authored by DaSo on 06/11/2013, Last Edited by DaSo on 06/11/2013
Related ranges: Unity Pro - SoCollaborative software
Was this helpful?
What can we do to improve the information ?