Technical FAQs

Ask a Question

Preventa XU - XUSLBR5A0520 has the error code 23, which it´s not at user´s manual. What´s the meaning of this error and how to solve it?

The error code 23 or starting by 2* cannot be displayed on the XUSLB/D type 4 curtains. Please check which is the correct error and use the XUSLB/D user manual to diagnostic and solve the issue in the application. Probably that the customer sees "23" error code instead of "32" error code on the IBI's (individual beam indicator).


Legacy KB System (APS) Data: RESL211723 V1.0, Originally authored by JeLe on 06/09/2013, Last Edited by JeLe on 06/09/2013
Related ranges: Preventa XU
Was this helpful?
What can we do to improve the information ?