Technical FAQs

Ask a Question

What is the part number for the Modbus Plus punch / insertion tool for pressing wires into the 990NAD23000 tap terminals?

The Modicon part number is 043509383.
The tool is manufactured by AMP Incorporated, P.O. Box 3608, Harrisburg, PA 17105-3608. Their part number is 552714-3.


Legacy KB System (APS) Data: RESL211719 V1.0, Originally authored by RoAl on 06/08/2013, Last Edited by RoAl on 06/08/2013
Related ranges: Modbus Plus
Was this helpful?
What can we do to improve the information ?