Technical FAQs

Ask a Question

What is a Lexium MDrive and who supports it?


The Lexium MDrive motion control is an integrated step motor + driver + programmable controller with choice of two motor sizes, NEMA 23 & 34, each with three lengths providing holding torque of 103 to 242 oz-in or 336 to 920 oz-in respectively. For example, LMDCM571, which is an MDrive comes in two versions - pulse/direction ( motor+drive) and motion control (motor+drive+controller) for direct programming with 11,120 bytes of flash memory.

Lexium MDrives are supported by SE Motion Tech Support ( formerly known as Intelligent Motion Systems IMS). They can be contacted via phone at (860) 295-6102 and via email at

Legacy KB System (APS) Data: RESL211704 V1.0, Originally authored by TVe on 06/07/2013, Last Edited by TVe on 06/07/2013
Related ranges: Other Motion controllers
Was this helpful?
What can we do to improve the information ?