Technical FAQs

Ask a Question

When I convert a variable using the Word_To_Real block my result appears be somewhat less than expected. Is this condidered to be normal behaviour ?

Yes, its normal behaviour and consistent with IEC standards. Please see attached. Word Conversion.pdfWord Conversion.pdf


Legacy KB System (APS) Data: RESL211688 V1.0, Originally authored by DaSo on 06/05/2013, Last Edited by DaSo on 06/05/2013
Related ranges: Unity Pro - SoCollaborative software
Was this helpful?
What can we do to improve the information ?