Technical FAQs

Ask a Question

Is there a Demo software package for the Magelis XBTGT terminals?

There is no demo package for these HMI terminals. The only option is to purchase Vijeo Design and register it. Part number for Vijeo Design software is
VJDSNDTGSV61M.


Legacy KB System (APS) Data: RESL211610 V1.0, Originally authored by TVe on 05/30/2013, Last Edited by TVe on 05/30/2013
Related ranges: Magelis XBT GT
Was this helpful?
What can we do to improve the information ?