Technical FAQs

Ask a Question

What are the causes for a n02 warning or a F02 error on a Lexium 17D drive?

A n02 warning can be reported if the power threshold set by the parameter "Max Regen Power" is exceeded.
A F02 error is reported if the DC Voltage limit is exceeded. The user manual for Lexium 17D drive provides possible causes and/or correction action for this and other faults.


Legacy KB System (APS) Data: RESL211608 V1.0, Originally authored by TVe on 05/30/2013, Last Edited by TVe on 05/30/2013
Related ranges: Lexium 17D
Was this helpful?
What can we do to improve the information ?