Technical FAQs

Ask a Question

Can you change the amount of diagnostic registers in the Profibus 140CRP81100 module when using Momentum I/O and Concept?

Goals and Symptoms

To go over the diagnostics for configuring the amount of diagnostic registers.

Causes and Fixes

Once you go and import the .cnf file for the exported Sycon file into the Concept program, the default diagnostic length is 6. If you want more diagnostic registers for this you will do the following.


Changed from 6 to 13. The reference number will now go from 300020 to 300032.


Legacy KB System (APS) Data: RESL211593 V1.0, Originally authored by DiSa on 05/29/2013, Last Edited by DiSa on 05/29/2013
Related ranges: Modicon Quantum
Was this helpful?
What can we do to improve the information ?