Technical FAQs

Ask a Question

Does the Quantum 140ACO02000 analog output module supply power to the outputs?

No, the 140ACO02000 analog output module does not supply power to the outputs. It requires an external supply to power the outputs and it can be wired with a loop supply and wired either as a sink or source output.

Legacy KB System (APS) Data: RESL211568 V1.0, Originally authored by DiSa on 05/24/2013, Last Edited by DiSa on 05/24/2013
Related ranges: Modicon Quantum
Was this helpful?
What can we do to improve the information ?