Technical FAQs

Ask a Question

Is cable part number SC902 still valid?

SC902 is a Smart cable for Sy/Max made by Niobrara research and development ( NR&D) for short based in Joplin, MO. The cable part number is good and it should be still be available. Please contact NR&D directly at (800) 235-6723.


Legacy KB System (APS) Data: RESL211567 V2.0, Originally authored by TVe on 05/24/2013, Last Edited by TVe on 05/28/2013
Related ranges: Sy/Max
Was this helpful?
What can we do to improve the information ?