Technical FAQs

Ask a Question

Is there a way to read the FLTHIST and FLTCNT parameters from a Lexium 15 drive using CanOpen?

There are no corresponding CAN objects for reading FLTHIST and FLTCNT, but there some other CAN objects that may be used.

1001:00h -> Error register according to DS301
1002:00h -> Manufacturer status register
1003:00h -> Number of recorded errors
1003:01h -> Most recent error
2070:16h -> ERRCODE error register


Legacy KB System (APS) Data: RESL211564 V1.0, Originally authored by TVe on 05/24/2013, Last Edited by TVe on 05/24/2013
Related ranges: CANopen, Lexium 15
Was this helpful?
What can we do to improve the information ?