Technical FAQs

Ask a Question

What is the difference between these two integrated drive models - ILS1W853PB1A0 and ILS1U853PB1A0?

The difference is in the signal level of the communication interface.
ILS1W853PB1A0 - pulse/direction 5 V RS 422
ILS1U853PB1A0 - pulse/direction 24V, opto-isolated.

The above are fixed and cannot be changed by a dip switch setting or any other way.


Legacy KB System (APS) Data: RESL211563 V1.0, Originally authored by TVe on 05/24/2013, Last Edited by TVe on 05/24/2013
Related ranges: Lexium ILA, ILE, ILS
Was this helpful?
What can we do to improve the information ?