Technical FAQs

Ask a Question

What is the HTS code for a Quantum Analog Output module bearing part number 140ACO13000?

HTS stands for Harmonized Tariff Schedule. This reference is needed for International Trade purposes.
The HTS code for a Quantum Analog output module 140ACO13000 is 8538.90.80.60


Legacy KB System (APS) Data: RESL211562 V1.0, Originally authored by TVe on 05/24/2013, Last Edited by TVe on 05/24/2013
Related ranges: Modicon Quantum
Was this helpful?
What can we do to improve the information ?