Technical FAQs

Ask a Question

Do you need to have the Solution Extension for SoMachine installed to be able to program a XBTGC2000 series with a XBTGCCAN CANopen Master module?

No, you do not need the Solution Extension to program a a XBTGC2000 series with a XBTGCCAN CANopen Master module. Only the XBTGCCANS0 CANopen Master module requires SoMachine to have the Solution Extension installed on your computer.


Legacy KB System (APS) Data: RESL211559 V1.0, Originally authored by TVe on 05/24/2013, Last Edited by TVe on 05/24/2013
Related ranges: Magelis XBT GC, SoMachine
Was this helpful?
What can we do to improve the information ?