Technical FAQs

Ask a Question

What is the replacement for a Twin Line Stepper drive bearing p/n TLD0112F23111?

The Twinline TLD stepper drive has been de-commercialized and hence not available any more.
The replacement for a TLD0112F23111- Stepper drive without rotation monitoring is SD326DU25S2.


Legacy KB System (APS) Data: RESL211555 V1.0, Originally authored by TVe on 05/24/2013, Last Edited by TVe on 05/24/2013
Related ranges: Twin Line SER-TLC-TLD
Was this helpful?
What can we do to improve the information ?