Technical FAQs

Ask a Question

What is the replacement part number for AGOKIT018M075?

AGOKIT018M075 is a power cable for BPH075x, 095x and 115x motors. This cable kit used a AGOCAV004 cable which is a (4x1.5mm^2+(2x1mm^2) shielded cable. Motor side connector was AMOCON004D and Drive side connector was AEOCON009.
All parts are obsolete. As an alternative the VW3 M5301R1000 (currently available in Lex 32 part range) which is 100 m long can be used to make the power cable.

Was this helpful?
What can we do to improve the information ?