Technical FAQs

Ask a Question

What does Error E 1300 mean on a Lexium 05 drive?

Goals and Symptoms

This resolution serves to explain what error code E1300 means on a Lexium 05 drive?

Causes and Fixes

If the Lexium 05 drive displays an error "E1300" it normally means, that the PWA and PWB inputs were switched to LOW signal when the Drive was in status "Operation enabled" (Status 6).
However if the drive displays (dis) the PWA and PWB inputs were switched to LOW signal when the Drive was in status 4 (ready to switch on, disabled).

This error is not dependent on the HALT-Signal. If the HALT input was activated when the drive is still in status 6 (Operation Enabled), if the PWA and PWB inputs are switched to LOW, the drive will disable and Error E1300 will be reported.

Was this helpful?
What can we do to improve the information ?