Technical FAQs

Ask a Question

What is the replacement for Berger Lahr VRDM motor bearing part number 52627035000?

The type code for the VRDM stepper motor 52627035000 is a VRDM3913/50LWB 00IP4100D40730000000.
The replacement part number reference for this motor is BRS39BW470ABA.


Legacy KB System (APS) Data: RESL211478 V1.0, Originally authored by TVe on 05/17/2013, Last Edited by TVe on 05/17/2013
Related ranges: Other Motion controllers
Was this helpful?
What can we do to improve the information ?