Technical FAQs

Ask a Question

Is modifying the code in a Unity SFC chart allowed in online mode?

No, although the SFC chart can be modified in online mode, the user must go offline to Build the application.


Legacy KB System (APS) Data: RESL211469 V1.0, Originally authored by DaSo on 05/16/2013, Last Edited by DaSo on 05/16/2013
Related ranges: Unity Pro - SoCollaborative software
Was this helpful?
What can we do to improve the information ?