Technical FAQs

Ask a Question

Is there anything available for the SFW50 software that will make it run on a Pentium base PC?

The only thing you can try is SLOWDOS (see attachment) and you will need to run this .bat file in a DOS shell. It is recommended that you use a PC that is a 486 66MHZ or slower.
SLO.ZIP


NOTE:  The Symax software was obsoleted in 2012 and the recommended replacement for the hardware ans software is the M221 with SoMachine Basic software
Was this helpful?
What can we do to improve the information ?