Technical FAQs

Ask a Question

What is the TSX Momentum battery service life once the battery low indication comes on?

The TSX Momentum service life of a battery <30 days from the time a battery-low indication is received to actual battery failure @ 40 degrees C maximum ambient temperature with the system continuously powered down.


Note: The Momentum with the option adapter with the battery is obsolete and has been replaced ith the Unity Momentum processors and they have a super cap to hold the clock that is built in.
Was this helpful?
What can we do to improve the information ?