Technical FAQs

Ask a Question

What is the part number for the SOMachine software for the M258 controllers?

The following part numbers are applicable for version 3.1 of SoMachine Software.
These apply to the following M258 controllers.

TM258LD42DT, TM258LF42DT, TM258LD42DT4L, TM258LF42DT4L, TM258LF42DR, TM258LF66DT4L

SoMachine Solution Extension for Solution Controllers (2 DVDs)

MSDCHLLMUV31S0 - Single license
MSDCHLLMTV31S0 - Team License (10)
MSDCHLLMFV31S0 - Facility License (100)


Legacy KB System (APS) Data: RESL211338 V1.0, Originally authored by TVe on 05/02/2013, Last Edited by TVe on 05/02/2013
Related ranges: SoMachine
Was this helpful?
What can we do to improve the information ?