Technical FAQs

Ask a Question

Why is my NEMA 4x outdoor enclosure painted white?

As of5/1/2013, all NEMA 4X factory assembled outdoor enclosures are now white painted aluminum rather than gray painted steel. The new white enclosures are an improvement over the old enclosures for a number of reasons. The white paint reflects more of the sun's heat and the fact that they are aluminum results in the enclosures being corrosion resistant, lighter, and recyclable.
Key Words:
Factory Assembled Enclosures, Nema 4, 4X , grey, gray


Legacy KB System (APS) Data: RESL211315 V1.0, Originally authored by MaTh on 05/02/2013, Last Edited by MaTh on 05/02/2013
Related ranges: Other Enclosures
Was this helpful?
What can we do to improve the information ?