Technical FAQs

Ask a Question

Can a Twido TWDLCAA40DRF controller have a Memory cartridge and a Real Time Clock chip (RTC) installed?

Yes. The Twido TWDLCAA40DRF has a "built-in" RTC chip so you do not need to add the chip. As for the memory chip, this would only be needed if you want to save the program to it and it would not remain in the controller. It also has an option to add an external battery to hold the program when it is powered down.


Legacy KB System (APS) Data: RESL211300 V1.0, Originally authored by DiSa on 05/02/2013, Last Edited by DiSa on 05/02/2013
Related ranges: Twido
Was this helpful?
What can we do to improve the information ?