Technical FAQs

Ask a Question

Can the Fiber port on the Unity Quantum 140CPU67160 be used to communicate to Ethernet Modbus TCP devices?

No. The native Ethernet port is a 100 Mbps fiber optic link. It is dedicated to Hot Standby . In order to communicate "Ethernet Modbus TCP" an NOE card will be required in your configuration.

Legacy KB System (APS) Data: RESL211205 V1.0, Originally authored by RoAl on 04/12/2013, Last Edited by RoAl on 04/12/2013
Related ranges: Modicon Quantum
Was this helpful?
What can we do to improve the information ?