Technical FAQs

Ask a Question

What is the replacement for the Advantys STBDDO3600 digital output module?

The replacement is the STBDDO3600K. The "K" at the end of the part number designates kit. The kit now contains module, base and appropriate number of both spring and screw type connectors.


Legacy KB System (APS) Data: RESL211064 V1.0, Originally authored by RoAl on 03/27/2013, Last Edited by RoAl on 03/27/2013
Related ranges: Modicon STB
Was this helpful?
What can we do to improve the information ?