Technical FAQs

Ask a Question

Is there a screw type version of the terminal blocks (BMXXTSHSC20) required for the BMXEHC0200 high speed counter module ?

No, the only option for the BMXEHC0200 high speed counter module is the BMXXTSHSC20. It includes (2) 16-terminal spring clamp connectors and (1) 10-terminal spring clamp connector.


Legacy KB System (APS) Data: RESL211034 V1.0, Originally authored by DaSo on 03/23/2013, Last Edited by DaSo on 03/23/2013
Related ranges: Modicon M340
Was this helpful?
What can we do to improve the information ?